Green Hills 7.1.6 Creat a project Debug to MPC5746C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Green Hills 7.1.6 Creat a project Debug to MPC5746C

785 次查看
lianwu
Contributor I

 Hi,

      i am now using the Green Hills 7.1.6 Creat a project of MPC5746C(default hello project), and using TRACE32 Download the project to MPC5746C, but the projcet can't run to Main Function.  

      so i think  there has some problem of startup. what the step of creat a new project of MPC5746C when Using GHS 7.1.6. and i download the example project : Example-MPC5646C-PIT-ISR-v1_0-GHS614(MPC5 software example list ),but is also can't run to main function.

     when i creat a new project of MPC5746C, how do i creat or use the starup files.  

1 回复

524 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

What does it mean, can't run into main?

Do you get exception, stuck in loop waiting for the flag, or reset, etc...?

What about clocks? Are you using IRC, external crystal, pll?

Do you have same crystal as in examples?

With the information you have provided to use it is impossible to help you.

Peter