FLASH ECC Error Injection on MPC5744P question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLASH ECC Error Injection on MPC5744P question

1,299件の閲覧回数
kai-hsiangtu
Contributor I

davidtosenovjan‌

Hello David,

I've try example project provide by S32DS about ECC error injection on MPC5744P and it works fine when I built it without optimization... 

Once I try it with any kind of optimization, FCCU_Alarm_Interrupt and Machine_check_handler won't be trigger and the message window only show "End of MPC5744P ECC error test." after I select injection option.

How should I do if I need to implement this ECC feature with optimization build option?

Best regards,

Wally

タグ(2)
0 件の賞賛
返信
0 返答(返信)