Enet_rmii_udp Transmit Problem 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enet_rmii_udp Transmit Problem 

1,278 Views
876152220
Contributor II

Hi,
I am using MPC5748G enet_rmii_udp example code on s32 design studio IDE.
When I send data less than 12 bytes, it can work and PC can receive. But if it more than 12 bytes, the PC can not receive.
I check the code many times, and I can not find why it does so. Is there anyone can help me to solve the problem.Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,216 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I think the frame lengths are not properly defined in the example. Try the modification as per the ethernet example enet_rmii_upd 

BR, Petr

0 Kudos
Reply