HI everyone,
I am using MPC5748G processor for a certain application and using Trace32 Lauterbach for debugging and flashing. My problem is that when my application resets the core multiple times, the processor goes in a state where it has to be power-cycled, and simply resting the target doesn't work.
meanwhile the debugger lists this error message :
" system.up error: received invalid OSR (0x000)
- does the target assert JCOMP while RESET is asserted?
- is the device censored?
error: received invalid OSR while core running (0x000) "
I have tried :Tools - Halt core at power-on reset. But there is no cmm file found for this
so is it a hardware limitation or is there any script that can help me solve this problem ?
Looking forward reply,
Hi,
it is caused by reset escalation feature:
The script for "Halt core at power-on reset" is attached. But you have to do power off-on cycle in any case.
It is necessary to find the source of reset. You can check it in RGM_FES and RGM_DES registers. It is usually caused by watchdog.
Regards,
Lukas
lukaszadrapa For now i have tried the cmm file (it tell me to power on/off) but after that i get the following
error: ERROR while releasing RESET: timeOut
Is there anything to do in this case or any other scripts that i can try
thanks
Hi,
I would really appreciate if you do not multiply the threads.
Peter