Could not reset / or attach MPC5748G  in trace32 using JTAG debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not reset / or attach MPC5748G  in trace32 using JTAG debugger

2,011 Views
chfakhtchfakht
Contributor III

HI everyone,

 

I am using MPC5748G processor for a certain application and using Trace32 Lauterbach for debugging and flashing. My problem is that when my application resets the core multiple times, the processor goes in a state where it has to be power-cycled, and simply resting the target doesn't work.

 

meanwhile the debugger lists this error message :

"    system.up error: received invalid OSR (0x000)

                                - does the target assert JCOMP while RESET is asserted?

                                - is the device censored?

     error: received invalid OSR while core running (0x000) "

 

 

I have tried :Tools - Halt core at power-on reset.  But there is no cmm file found for this

so is it a hardware limitation or is there any script that can help me solve this problem ?

 

Looking forward reply,

Labels (1)
3 Replies

1,301 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it is caused by reset escalation feature:

pastedImage_0.png

pastedImage_1.png

The script for "Halt core at power-on reset" is attached. But you have to do power off-on cycle in any case.

It is necessary to find the source of reset. You can check it in RGM_FES and RGM_DES registers. It is usually caused by watchdog.

Regards,

Lukas

1,301 Views
chfakhtchfakht
Contributor III

lukaszadrapa For now i have tried  the cmm file (it tell me to power on/off) but after that i get the following

error: ERROR while releasing RESET: timeOut

Is there anything to do in this case or any other scripts that i can try

thanks

0 Kudos

1,301 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I would really appreciate if you do not multiply the threads.

Peter