CW2.10,My design use SPC5605bmll6,When debuging,if CPU setting is autodetect,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).
If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B.While I Add Register in Variables window,it is all MPC5607B register.
1. I what to know that is OK or not.
2.At the same time,In project I cannot change all PCR.R.but In memory window,I can write data in sram(0x40000000).and ex-clock is OK.
need help
THANKS
Hello,
what do you mean by:
Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).
If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B
Where did you check that this algorithm was used?
About your second question, please read my answer in your second thread:
https://community.nxp.com/thread/445957
Regards,
Martin