Dear Team:
I'm trying all the 6 CAN modules of 5606B with XPC56XX EVB (mother board + daughter card), but unfortunately my code (based on AN2865) only works on CAN_0 (PB0/PB1), CAN_2 (PE8/PE9 and PF8/PF9), CAN_3 (PC5/PC4, PF8/PF9 and PE8/PE9). Could you give me an example of how to use CAN_1, CAN_4 and CAN_5?
Thank you.
Solved! Go to Solution.
Hi,
example will be the same, just be sure pins are properly initialized and connected to the transceiver.
Also check if nothing else is connected to TX/RX lines, that can influence signals..
BR, Petr
Hi,
example will be the same, just be sure pins are properly initialized and connected to the transceiver.
Also check if nothing else is connected to TX/RX lines, that can influence signals..
BR, Petr