********************************************************************************
* Detailed Description:
* This example shows, how to use overlay feature - how to remap SRAM over Flash.
* The remapping is visible only in mirrored flash address space. Normal address
* space is not affected.
* To see effect of the remapping, read the comments and watch following
* addresses in debugger before and after executing Overlay() function:
*
* SRAM over Flash test case:
* 0x4003_0000
* 0x090C_0000
*
* Test HW: X-MPC5744PE257DC, MPC57xx motherboard
* MCU: PPC5744PFMMM8 1N65H
* Fsys: 200 MHz
* Debugger: Lauterbach Trace32
* Target: internal_FLASH (debug mode, release mode)
* EVB connection: none
*
********************************************************************************