Example MPC5643L 2b RAM and 2b FLASH ECC error injection CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5643L 2b RAM and 2b FLASH ECC error injection CW210

Example MPC5643L 2b RAM and 2b FLASH ECC error injection CW210

********************************************************************************

* Detailed Description:

* Purpose of the example is to show how to generate Multi bit ECC error in

* internal SRAM or FLASH (user must choose it in the option at the end of main

* function) and how to handle this error with respect to constraints given by

* MPC5643L architecture (ECSM/RGM/FCCU relation and ECC error handling through

* reset). The example is only possible to run in internal_FLASH target. Power-

* -on-reset is required after downloading the code into MCU's flash. The example

* displays notices in the terminal window (setting specified below). No other

* external connection is required.

* ------------------------------------------------------------------------------

* Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon

* Target :         internal_FLASH

* Fsys:            120 MHz PLL0

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0

* EVB connection:  default

*

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎08-21-2014 08:01 AM
更新者: