EXAMPLE_MPC5777C_CORE_WATCHDOG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EXAMPLE_MPC5777C_CORE_WATCHDOG

EXAMPLE_MPC5777C_CORE_WATCHDOG

********************************************************************************

* Detailed Description:

* Example of core watchdog implementation on Cobra 55. It executes on core 0

* All the functions are in the file "watchdog.c"

*WatchDogCreate(delay, FirstTimeout, SecondTimeout) -> create/configure the wathdog timer

*WatchDogStart() -> start the watchdog timer

*WatchDogService() -> acknowledge the watchdog timer

* ------------------------------------------------------------------------------

* Test HW:         MPC5777C-416DS Rev.A + MPC57xx MOTHER BOARD Rev.C

* MCU:             PPC5777CMM03 2N45H CTZZS1521A

* Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz

* Debugger:        Lauterbach Trace32

* Target:          internal_FLASH

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎12-13-2016 09:57 AM
更新人: