I have success compiled demo project "aws_remote_contril_enet", but when I run it, it failed at certificate,
because demo project try to read/write flash for access the certificate files
my question is how to modify the project let it read certificate from:
"aws_clientcredential_keys.h"
static const char clientcredentialCLIENT_CERTIFICATE_PEM[]
and more how to disable flash read/write ?
Hi, Kerry,
I have sloved problem of above, but I got a new problem:
If I put "aws_examples/remote_control_enet"
and
"K66F_demo_apps_lwip_lwip_httpssrv_mbedTLS_freertos"
two project together, then the normal "http" service is ok, but "WEBSocket example" doesn't work, please let me know how to setup lwip? or may be some thing conflict with these two project?
Hi Changfu,
Actually, the remote control step is a little complex, you said you solved the problem, do you missed some configuration in the aws side?
You said your new problem is caused by the mix of two project, how you put it works together, in your new project, if you comment the aws, whether your lwip can work normally?
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank for replay
first, I have setup aws iot correctly, and I can subscribe and publish topic
second, if I start aws iot task, the lwip and http service are working fine, except WEBsocket doesn't work only
other else same as "cgi" "ssi" are working fine
Hi Changfu Zhao,
Please tell me what the NXP chip or the board you are using?
I need to check the according SDK, because we don't have the directly sdk name as SDK_2.3.1 aws iot .
Please tell me the board or chip you are using, then we will help you to check it.
Waiting for your reply!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Kerry,
The demo project inside SDK_2.3.1_MK66FX1M0xxx18_MCUX.zip
.. /boards/frdmk66f/aws_examples/remote_control_enet
You can build it from SDK builder
Thank you very much
Thanks for your updated information, I will test it on my side, please wait patiently.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank very much
Hi, Kerry Zhou,
My chip is MK66FX1MVLQ18, you can to use FRDM_K66f to test with demo project “aws_remote_control_enet”
I found some problem, the code was designed for LPC chip, the config of flash driver is wrong
My second question is the readme.txt in this demo project not detail for how to setup aws iot,
And more, do you have App run in cell phone for test?
Thank you very much
Hi Changfu,
You still didn't let me know where you download aws_remote_control_enet?
Please give me the code link, I will test it on my side.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Kerry,
The demo project inside SDK_2.3.1_MK66FX1M0xxx18_MCUX.zip
.. /boards/frdmk66f/aws_examples/remote_control_enet
You can build it from SDK builder
Thank you very much