Hello guys,
I got an issue since the switch to SDK 2.4 project. For now I was using the exemples released in A71CH Software Package. I heard that it was integrated onto SDK 2.4 so I imported the project with MCUXpresso 10.2.
My issue is that when starting the project an HardFault_Handler pop out at the start of the scheduler of FreeRTOS.
I didn't touch anything. I'm runnign it on a FRDM-K64F rev E board with the A71CH arduino compatible shield OM3710/A71CHARD.
Hi Theophile Leroy
Do you have errors just in those 2 example codes? Using the same SDK and IDE that you have, I have tried them in my frdm-K64F SCH-REV-D1 and I don't see any problem in them. I will try to use the exact Schematic revision that you have and if I find something I will let you know.
Best regards
Jorge Alcala
Ok solved the issue by switching to SDK 2.4.1. Project is working fine on this one. I don't know where the error come form... Maybe not a big deal.
Thank you for help