SDK 2.0 Builder Missing Files !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK 2.0 Builder Missing Files !

2,922 次查看
mesbahuddinmoha
Contributor I

Hello, i am building SDK for  MK22FN1M0VLH12 (MK22FN1M0xxx12) micro-controller using the online SDK builder. I think there is a bug as i can not see the "fsl_clock" being generated !! this prevents me from compiling . Any Help ?

pastedImage_1.png

0 项奖励
回复
7 回复数

2,720 次查看
mesbahuddinmoha
Contributor I

Thnaks for the response ... yes i have copied the :

SDK_2.0_MK22FN1M0xxx12\devices\MK21FA12\drivers\fsl_clock.c

SDK_2.0_MK22FN1M0xxx12\devices\MK21FA12\drivers\fsl_clock.h

to the drivers files in my project ... the compilation is successful but the code is stuck at the following location indicating unsuccessful clock configuration  :

pastedImage_1.png

I have used the KINETIS Expert to generate the .clock settings :

pastedImage_2.png

I have used SDK 2.0 on FRDM K64 sucessfully but on this chip it seems the SDK is not ready or its not compatible.

0 项奖励
回复

2,720 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Uddin,

- Ok, I will tell you .ASAP when I get the workaround.

- About the clock configuration,  how do you know it is also have some problem, does it

can not work when you copy the code into your project ?

Thanks for your sharing .

BR

ALice

0 项奖励
回复

2,720 次查看
mesbahuddinmoha
Contributor I

After copying the clock configuration files in to the project the proceed to compilation but as i run in debug mode it gets stuck at the point i have shown in my previous post. The code doesn't proceed any further just blocks at the while loop.

I do not doubt the board as i can do the clock configuration and run the project normally when i do a PE (Processor Expert) project !! This is stopping me from using the SDK 2.0.

0 项奖励
回复

2,720 次查看
Lukas_Heczko
NXP Employee
NXP Employee

Hi Mesbah, Alice,

this issue is already fixed in the latest version available on https://mcuxpresso.nxp.com.

Lukas

2,720 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lukas

OK, thank you very much !

BR

Alice

0 项奖励
回复

2,720 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mesbah,

OK, the key problem is the SDK code , I will reply you .ASAP.

BR

Alice

0 项奖励
回复

2,720 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mesbah,

I will report this bug to MCUXpresso SDK team  , sorry for the inconvenient to you .

There is the clock functions file about MK21F12, maybe you can refer to it to develop

before I got the fix .

SDK_2.0_MK22FN1M0xxx12\devices\MK21FA12\drivers\fsl_clock.c

BR

Alice

0 项奖励
回复