Hi everyone,
I'm using a custom board based on RT1064, with MCUXpresso 11.8.0 and SDK 2.12.0.
The board uses a LAN8720A ethernet tranceiver that is working fine.
I have a trouble when the system starts with then LAN cable disconnected: if I connect the cable after the init is completed, a ping packet from another device is not answered.
Here is a summary of my code:
tcpip_init( NULL, NULL );
...
netif_add( &NetIfLAN, &IPAddress, &NetMask, &DGAddress, &EthConfig, ethernetif0_init, tcpip_input );
netif_set_default( &NetIfLAN );
StartNetworkSupervisor();
void NetWorkSupervisor( void )
{
bool link, oldlink = false;
while( 1 )
{
if( PHY_GetLinkStatus( EthConfig.phyHandle, &link ) != kStatus_Success )
link = false;
if( link != oldlink )
{
if( link != false )
{
PRINTF( "LINK UP\n" );
sys_lock_tcpip_core();
//netif_set_link_up( &NetIfLAN );
netif_set_up( &NetIfLAN );
sys_unlock_tcpip_core();
}
else
{
PRINTF( "LINK DOWN\n" );
sys_lock_tcpip_core();
//netif_set_down( &NetIfLAN );
netif_set_link_down( &NetIfLAN );
sys_unlock_tcpip_core();
}
oldlink = link;
}
...
}
}
In the terminal I can see the "LINK UP" and "LINK DOWN" strings, so the connection and disconnection events are handled. I tried both with and without the netif_set_link_up() and netif_set_link_down() calls, but the behaviour is the same.
Does anyone have some suggestion?
Many thanks
Biafra
Hello, my name is Pavel, and I will be supporting your case, I reviewed your comments, and I suggest reviewing the example on the SDK because there are some states in the protocol that need to wait. Maybe you could do a porting.
Best regards,
Pavel
Hi Pavel,
Many thanks for your answer.
I reviewed some example in SDK about LwIP, and I noticed that in freertos examples netifapi_netif_xxx functions are used.
So in my code I replaced the netif_xxx functions with the corresponding netifapi_netif_xxx functions, but the behaviour is the same.
In such examples I couldn't find the states to wait you mentioned: can you give me some details about them?
Many thanks
Biafra
Hello, sorry for the late response I apologize for the last response I was not clear; I recommend reviewing how the examples work they have a blocking mode of wait state until connecting the LAN cable.
Best regards,
Pavel
Hi @Pavel_Hernandez,
Many thanks for your answer.
Sorry for my my lack of clarity, I'll try to explain myself better.
The blocking mode have a configurable max numer of attempts (ENET_ATONEGOTIATION_TIMEOUT) to wait until connecting the LAN cable. If I connect the LAN cable before the number of attempts reaches ENET_ATONEGOTIATION_TIMEOUT the system works fine.
The system doesn't work if I connect the LAN cable after the max numer of attempts is reached.
The NetWorkSupervisor task is intended to recognize the cable connection/disconnection and to do the needed operartions to make the system work in all situations.
Many thanks
Biafra
Hi @Pavel_Hernandez,
Many thanks for your answer.
There isn't the NetWorkSupervisor() function in the examples, it's a function I've written thinking that it's needed to make the network work if it starts with the cable disconnected.
Many thanks
Biafra