Hi everyone,
I'm using a custom board based on RT1064, with MCUXpresso 11.8.0 and SDK 2.12.0.
The board uses a LAN8720A ethernet tranceiver that is working fine.
I have a trouble when the system starts with then LAN cable disconnected: if I connect the cable after the init is completed, a ping packet from another device is not answered.
Here is a summary of my code:
tcpip_init( NULL, NULL );
...
netif_add( &NetIfLAN, &IPAddress, &NetMask, &DGAddress, &EthConfig, ethernetif0_init, tcpip_input );
netif_set_default( &NetIfLAN );
StartNetworkSupervisor();void NetWorkSupervisor( void )
{
bool link, oldlink = false;
while( 1 )
{
if( PHY_GetLinkStatus( EthConfig.phyHandle, &link ) != kStatus_Success )
link = false;
if( link != oldlink )
{
if( link != false )
{
PRINTF( "LINK UP\n" );
sys_lock_tcpip_core();
//netif_set_link_up( &NetIfLAN );
netif_set_up( &NetIfLAN );
sys_unlock_tcpip_core();
}
else
{
PRINTF( "LINK DOWN\n" );
sys_lock_tcpip_core();
//netif_set_down( &NetIfLAN );
netif_set_link_down( &NetIfLAN );
sys_unlock_tcpip_core();
}
oldlink = link;
}
...
}
}
In the terminal I can see the "LINK UP" and "LINK DOWN" strings, so the connection and disconnection events are handled. I tried both with and without the netif_set_link_up() and netif_set_link_down() calls, but the behaviour is the same.
Does anyone have some suggestion?
Many thanks
Biafra
Hello, my name is Pavel, and I will be supporting your case, I reviewed your comments, and I suggest reviewing the example on the SDK because there are some states in the protocol that need to wait. Maybe you could do a porting.
Best regards,
Pavel
Hi Pavel,
Many thanks for your answer.
I reviewed some example in SDK about LwIP, and I noticed that in freertos examples netifapi_netif_xxx functions are used.
So in my code I replaced the netif_xxx functions with the corresponding netifapi_netif_xxx functions, but the behaviour is the same.
In such examples I couldn't find the states to wait you mentioned: can you give me some details about them?
Many thanks
Biafra
Hello, sorry for the late response I apologize for the last response I was not clear; I recommend reviewing how the examples work they have a blocking mode of wait state until connecting the LAN cable.
Best regards,
Pavel
Hi @Pavel_Hernandez,
Many thanks for your answer.
Sorry for my my lack of clarity, I'll try to explain myself better.
The blocking mode have a configurable max numer of attempts (ENET_ATONEGOTIATION_TIMEOUT) to wait until connecting the LAN cable. If I connect the LAN cable before the number of attempts reaches ENET_ATONEGOTIATION_TIMEOUT the system works fine.
The system doesn't work if I connect the LAN cable after the max numer of attempts is reached.
The NetWorkSupervisor task is intended to recognize the cable connection/disconnection and to do the needed operartions to make the system work in all situations.
Many thanks
Biafra
Hello, sorry for the late response what is the example where you find that functions NetWorkSupervisor, I reviewed the httpsrv_freertos but I can't find this.
Best regards,
Pavel
Hi @Pavel_Hernandez,
Many thanks for your answer.
There isn't the NetWorkSupervisor() function in the examples, it's a function I've written thinking that it's needed to make the network work if it starts with the cable disconnected.
Many thanks
Biafra
Hello, sorry but I´m afraid there is no nothing like this, I suggest creating a task supervisor to avoid using the counter.
Best regards,
Pavel