K81 with QSPI/XIP and high IRQ rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K81 with QSPI/XIP and high IRQ rate

Jump to solution
1,322 Views
alexklupsch
Contributor III

Hi,

i have a K81 with QSPI and some ADC code that should run from the QSPI. 

My first test gives some strange results, from internal flash averything runs ok, but when i move the IRQ handler to QSPI a simple LPUART communication lost some characters, sometimes.

My question is, can i run any code, even a high rate IRQ handler, from QSPI (XIP) without influence other stuff?

BR

Alex

1 Solution
1,160 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Alex,
The max QSPI AHB buffer is 512 byte. If you can't put all the LPUART service code in AHB buffer, every "missed" access to the buffer causes the controller to clear the buffer and fetch QSPI_BUFxCR[ADATSZ] amount of data from the serial flash. If this happens in a high frequency, the average instruction execution speed could be slower than you image. So my suggestion is put those speed sensitive code in internal flash, or use DMA.

Regards

Jing

View solution in original post

2 Replies
1,160 Views
alexklupsch
Contributor III

Hi Jing,

thank's for the info.

BR

Alex

0 Kudos
Reply
1,161 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Alex,
The max QSPI AHB buffer is 512 byte. If you can't put all the LPUART service code in AHB buffer, every "missed" access to the buffer causes the controller to clear the buffer and fetch QSPI_BUFxCR[ADATSZ] amount of data from the serial flash. If this happens in a high frequency, the average instruction execution speed could be slower than you image. So my suggestion is put those speed sensitive code in internal flash, or use DMA.

Regards

Jing