Wire ACK Fault in DAP Access: Debugger won't run

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wire ACK Fault in DAP Access: Debugger won't run

1,035 次查看
jordiclos
Contributor I

I am trying to debug with MCUxpresso IDE v10.1 a gpio example (gpio_led_output) and when I try to debug it appears that error.

I also tryied to erase flash memory and reinstall the mbed driver for windows but the error still appearing.

Someone know how to solve it and debug correctly?

Thanksdebug problem.JPG

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

806 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

What OS / version are you running on?

Have you been able to successfully debug this board previously?

Can you also confirm which board you are using? [I presume from the example you are trying to debug that it is a TWR-KV11Z75M, but it would be good to confirm.] It might also be worth ensuring that the OpenSDA has the latest firmware in it (from http://www.nxp.com/opensda), or even trying the alternate firmware images for SEGGER / P&E rather than the mbed/CMSIS-DAP.

Regards,

MCUXpresso IDE Support