What needs to change when LPCXpresso project is imported into MCUXpresso?

cancel
Showing results for 
Search instead for 
Did you mean: 

What needs to change when LPCXpresso project is imported into MCUXpresso?

488 Views
anaseem
Contributor IV

I imported LPCXpresso project to MCUXpresso IDE.  In MUCXpresso IDE project settings I noticed following setting:

Should I change this setting to MCUXpresso Style?

What other settings need to change ?

Regards,

1 Reply

307 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Amer,

You can find more information about the difference between these two settings in the sections 17.10.1 and 17.10.2 in the MCUXpresso User guide. You might also find this post useful:

https://community.nxp.com/message/980370 

It is also recommended to delete the debug connections and let the MCUXpresso auto discovery functionality to create it again.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer