Our board has an RT1052 connected to a QSPI Flash W25Q512JV (so larger than default, and QSPI, not HyperFLASH) part.
What is the expected way to connect MCUXpresso to our board with the PEmicro Multilink Unversal FX?
If I use the LPC-Link2 instead, I can just select the RT1052-QSPI generic loader, and it seems to work fine.
But if I want to load FLASH via the Multilink FX - seems I need to do a few more things?
See screenshot:
解決済! 解決策の投稿を見る。
Hi @variable_andrew ,
No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.
Regards,
Jing
Hi @variable_andrew ,
No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.
Regards,
Jing
every time i try to launch with ^^^ - the console only provides the following output:
P&E Semihosting Console
Connection closed by the GDB server.