RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX

Jump to solution
1,044 Views
variable_andrew
Senior Contributor I

Our board has an RT1052 connected to a QSPI Flash W25Q512JV (so larger than default, and QSPI, not HyperFLASH) part.

What is the expected way to connect MCUXpresso to our board with the PEmicro Multilink Unversal FX?

If I use the LPC-Link2 instead, I can just select the RT1052-QSPI generic loader, and it seems to work fine.
But if I want to load FLASH via the Multilink FX - seems I need to do a few more things?

See screenshot:

MCUXpresso w PEmicro

0 Kudos
1 Solution
1,029 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @variable_andrew ,

No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.

jingpan_0-1653386684249.png

 

 

Regards,

Jing

 

View solution in original post

2 Replies
1,030 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @variable_andrew ,

No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.

jingpan_0-1653386684249.png

 

 

Regards,

Jing

 

1,043 Views
variable_andrew
Senior Contributor I

every time i try to launch with ^^^ - the console only provides the following output:

P&E Semihosting Console

Connection closed by the GDB server.

0 Kudos