Condition:
MCUXpresso IDE v11.0.0_2516
TWR-KV58F220M Tower System Development Board
host PC: Windows 10
connect host PC to target board (J22) via USB able
Issue:
Create a new project, build it. 0 error, 0 warning
But, when click Debug, following message displays in the <Probes discovered> window:
Connect to target: MKV58F1M0xxx24
No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target.
red LED () --- ON
orange LED --- ON
And, following messages display in the RedlinkServer window of MCUXpresso:
[Started Server]
[Connected on port 3025]
redlink> ProbeList
No probes found
But, host PC is connected to target TWR-KV58F220M (J22) via USB cable.
Hi
I would suggest you delete the existing launch configuration , then a debug probe discovery operation will be automatically performed to display the available debug connections.
Please refer to below link for more details.
MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery)
Regards
Daniel