MCUXpresso TWR-KV58F220M target connection issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso TWR-KV58F220M target connection issue

670 次查看
jxu
Contributor I

Condition:

MCUXpresso IDE v11.0.0_2516

TWR-KV58F220M Tower System Development Board

host PC: Windows 10

connect host PC to target board (J22) via USB able

Issue:

Create a new project, build it. 0 error, 0 warning

But, when click Debug, following message displays in the <Probes discovered> window:

Connect to target: MKV58F1M0xxx24

No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target.

red LED ()   --- ON

orange LED --- ON

0 项奖励
2 回复数

545 次查看
jxu
Contributor I

And, following messages display in the RedlinkServer window of MCUXpresso:

[Started Server]

[Connected on port 3025]

redlink> ProbeList

No probes found

But, host PC is connected to target TWR-KV58F220M (J22) via USB cable.

0 项奖励

545 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

I would suggest you delete the existing launch configuration , then a debug probe discovery operation will be automatically performed to display the available debug connections.

 

Please refer to below link for more details.

MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery) 

 

Regards

Daniel

0 项奖励