Is USB Device re-enumeration necessary on iMX6ULL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is USB Device re-enumeration necessary on iMX6ULL?

ソリューションへジャンプ
1,021件の閲覧回数
stephenbialkows
Contributor III

AN5385 says that re-enumeration is not necessary for MCUXpresso.  MCUXpresso doesn't support the cortex A cores.  But I wonder if the USB core is similar enough on the i.MX6ULL that re-enumeration is not necessary when coming out of low power mode (consistent with what is detailed in AN5385).

タグ(2)
0 件の賞賛
返信
1 解決策
914件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stephen

AN5385 describes USB device suspend state (defined by usb specification)

which is different from i.MX6ULL processor low power modes described in

Table 10-1. Low Power Mode Definition Reference Manual. In general case re-enumeration

is necessary in i.MX6ULL processor low power modes, as it can turn off processor modules.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
915件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stephen

AN5385 describes USB device suspend state (defined by usb specification)

which is different from i.MX6ULL processor low power modes described in

Table 10-1. Low Power Mode Definition Reference Manual. In general case re-enumeration

is necessary in i.MX6ULL processor low power modes, as it can turn off processor modules.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信