I can see from this:
#define FSL_FEATURE_UART_HAS_ADDRESS_MATCHING (1)
that there may be an address matching capability in the UART, but I don't see any documentation of its use in the API. Can someone point me to a more detailed set of documentation for the UART used in this SOC? Even better, any experience on here with enabling and using this feature?
HI Jeremy.
FSL_FEATURE_UART_HAS_ADDRESS_MATCHING is used in KSDK1.x SW package.
Normally it is defined in <mcu_name>_features.h file and used in fsl_uart_hal.c file.
it is to brief Supports two match addresses to filter incoming frames.
I just checked there is no document describing this MACRO.
KSDK1.3 API reference manual can be downloaded here:
http://www.nxp.com/docs/en/reference-manual/KSDK13APIRM.pdf
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Well it seems I must ask these questions before I find the answer. In this case:
http://www.nxp.com/docs/en/reference-manual/K66P144M180SF5RMV2.pdf
Hope this helps anyone stumbling along the same path.