Deployment of tflite model on MIMXRT1064 evaluation kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deployment of tflite model on MIMXRT1064 evaluation kit

829 Views
Emin
Contributor III

I have a baby cry detection tflite (tensorflow lite) file, which contains the model itself. How can I deploy this model to the MIMXRT1064-evk to run inference via MCUXpresso IDE. Can you suggest some tutorials and input dataset for baby cry detection?

0 Kudos
Reply
3 Replies

795 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Emin 

Can you be more specific with what you want to do with the RT1064, please? For me too look for tutorials or documents that can help you.

Best Regards, Miguel.

0 Kudos
Reply

785 Views
Emin
Contributor III

yes, I m looking for the implementation of tensorflow lite on the MCUs. I have attached some example tutorials that I found about glow and cmsis-nn. Additionally, there is a lack of tutorials for implementing sound detection models on tensorflow lite in the MCUs since RT1064 is not the only one I have to do testing(I need to do same task on LPC55S69)

0 Kudos
Reply

776 Views
Miguel04
NXP TechSupport
NXP TechSupport

Thank you @Emin 

This application note could help you, AN13065 Gender Voice Recognition with TensorFlow Lite Inference, please look into it.

Best Regards, Miguel.

0 Kudos
Reply