Hi,
I'm using McuXpresso ide (latest version: 10.2.1 [Build 795] [2018-07-25]) on Linux Ubuntu 16.04.
I'm using config tools integrated into the IDE.
I have created the project for MK20 Series controller. "Clocks" & "Pins" tools are working for me in the McuXpresso. I can generate code also. But "Peripherals" tool is not working.
When I open "Peripherals" tool then I get error "Corrupted MCU Data". Attached is a photo of the problem.
Can someone please tell me what have I missed while creating the project?
Any inputs will be of help.
Regards, Pj
解決済! 解決策の投稿を見る。
Hello,
the error message is misleading, the peripherals tool is not basically supported for the given processor (yet). It means you did not miss anything. In most cases the Pins and Clocks tools are supported for any processor, the Peripherals tool is the youngest tool and the support is added incrementally.
Regards,
Libor
Hi Pj,
Your issue is normal. "Config Tool - Peripherals" feature is not implement for MK20 yet.
Please see summary in this article
https://community.nxp.com/docs/DOC-333073
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ZhangJennie & liborukropec,
When will "peripherals tool" be available for MK20 series of processors?
Regards, Pj
No ETA yet. But I don't think it can be implemented in near future.
Jennie Zhang
Hello,
the error message is misleading, the peripherals tool is not basically supported for the given processor (yet). It means you did not miss anything. In most cases the Pins and Clocks tools are supported for any processor, the Peripherals tool is the youngest tool and the support is added incrementally.
Regards,
Libor