hot fix for KV5x using 50MHz external reference clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hot fix for KV5x using 50MHz external reference clock

hot fix for KV5x using 50MHz external reference clock

This tip will show you how to use MCUXpresso Config Tools V4.1 generate codes for KV5x with 50MHz external reference clock.

The fec_extal in datasheet shows that the maximum frequency of Input clock frequency (external clock mode) is 48MHz.

1 fec_extal 48MHz.png

It will lead code generation failed when you configure 50MHz as the external reference clock in latest MCUXpresso Config Tools V4.1. (Code generation in case of warnings shouldn't be blocked. It will be fixed for MCUXpresso Config Tools V5.)

2 Code generation failed. Files were not updated.png

Some customer had met this issue when using TWR-KV58F220M board, this board connect a 50MHz_OSC to EXTAL0.

50MHz OSCILLATOR TWR-KV58F220M.png

My colleague have prepared a hot fix for this issue (for all MKV5x MCUs). After install the attached hot_fix_MCUXpresso_Config_Tools_V4_1_data_MKV58_MCUCM-3936, customer is able to overcome it.(Notice: The ProgramData folder was hidden by default.)

3 hot_fix_Installation.png

4 Code successfully generated.png

附件
无评分
版本历史
最后更新:
‎09-30-2018 01:32 AM
更新人: