Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

ソリューションへジャンプ
843件の閲覧回数
bowerymarc
Contributor V
0 件の賞賛
返信
1 解決策
804件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
805件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

0 件の賞賛
返信
820件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bowerymarc 

 

Here is my test result based on Ubuntu22.04.

Please make sure you have updated and upgraded the Ubuntu packages.

Zhiming_Liu_0-1708992910021.png

Best Regards

Zhiming

 

0 件の賞賛
返信