Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

Jump to solution
1,013 Views
bowerymarc
Contributor V

Screenshot 2024-02-26 145637.png

0 Kudos
Reply
1 Solution
974 Views
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

View solution in original post

0 Kudos
Reply
2 Replies
975 Views
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

0 Kudos
Reply
990 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bowerymarc 

 

Here is my test result based on Ubuntu22.04.

Please make sure you have updated and upgraded the Ubuntu packages.

Zhiming_Liu_0-1708992910021.png

Best Regards

Zhiming

 

0 Kudos
Reply