Couldn't able to flash the binaries on the board FRDM-K82F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Couldn't able to flash the binaries on the board FRDM-K82F

656 次查看
sainathkonda
Contributor I

Couldn't able to flash the binaries on the board FRDM-K82F, it is working in debugger mode

Tried different methods in one method 

LPUART0 is blocked (no communication at all ) 

Used external debugger as well. still it needs a trigger from IDE

??

0 项奖励
回复
2 回复数

518 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the late reply!

Would you please tell us which IDE and external debugger are you using?

If you are using the on-board OpenSDAv2.2, the drop the bin file into MSD.

OpenSDAv2.2 FRDM-K82F.PNG

If you are using Segger J-Link, please refer the method in J-Link Flash Download.pastedImage_1.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

518 次查看
sainathkonda
Contributor I

Hi Robin

Thanks for responding

We used MCUxpresso and external debugger used was ULINK2 (by ARM).

We are using on board OpenSDA_FRDM-K82F, I didnt find any MSD  in OpenSDA.

But we solved the issue by making the board in semihost mode.

Why this board need a trigger always is it intentional??

0 项奖励
回复