HotFix: Vision Toolbox for S32V234 1.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HotFix: Vision Toolbox for S32V234 1.1.0

3,522 Views
paulvlase
NXP Employee
NXP Employee

HotFix_1: "No function or variable is defined 'FileName'" error in nxpvt_build()

 

Problem: When trying to run run_face_detection_camera_main.m

 

Root Cause: Coding building error

 

Workaround:  Update the files attached in the following folders 

 {install_dir}\internals\build\private\nxpvt_build.p
Labels (1)
0 Kudos
Reply
4 Replies

3,305 Views
jim_duan
Contributor II

I am using matlab R2018a. This hotfix doesn't work for it.

Thanks,

0 Kudos
Reply

3,306 Views
18502532079
Contributor I

well, the hot-fix seems not working, i encounter the same error When trying to run run_face_detection_camera_main.m

paulvlase

0 Kudos
Reply

3,306 Views
nxf40536
NXP Employee
NXP Employee

Hi 18502532079@163.com‌,

Can you please tell me which version of MATLAB you are using ? 

Thank you,

Vlad Dascau

0 Kudos
Reply

3,306 Views
Daniel_Popa
NXP Employee
NXP Employee

iulianbulancea‌ 

nxf40536

Please have a look!

Thanks!

Daniel

0 Kudos
Reply