BSP19.0 for S32V234 ERROR: glibc-initial-2.26-r0 do_configure: Function failed: do_configure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP19.0 for S32V234 ERROR: glibc-initial-2.26-r0 do_configure: Function failed: do_configure

2,160件の閲覧回数
2802911181
Contributor II

I encountered an error while building BSP19.0 for S32v234EVB, the log as below:

----------------------------------------------------------------------------------------------------------

$ bitbake virtual/kernel -c menuconfig
WARNING: Host distribution "ubuntu-18.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#################################################################################| Time: 0:00:00
Loaded 3423 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-fsl-linux"
MACHINE = "s32v234evb"
DISTRO = "fsl-auto"
DISTRO_VERSION = "1.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky
meta-yocto-bsp = "HEAD:c770664d3125a0a0e73444a3a2a97418b7c0d7a5"
meta-oe
meta-multimedia
meta-python
meta-networking
meta-gnome
meta-filesystems
meta-webserver
meta-perl
meta-xfce = "HEAD:6e3fc5b8d904d06e3aa77e9ec9968ab37a798188"
meta-virtualization = "HEAD:4277759428e96605b8dbe95a43891e217ae8d399"
meta-freescale = "HEAD:bf7fd9cfe0788fe2f819a4ae2cc7db8327fe161a"
meta-alb = "HEAD:79563288fea20bf8fcb09177c0c5b87cb8f2ba01"
meta-linaro-toolchain = "HEAD:30f0f5e158ba29c4b1ccfdd66f0368726e4179e0"

Initialising tasks: 100% |############################################################################| Time: 0:00:02
Checking sstate mirror object availability: 100% |####################################################| Time: 0:00:00
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: glibc-initial-2.26-r0 do_configure: Function failed: do_configure (log file is located at /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/temp/log.do_configure.648)
ERROR: Logfile of failure stored in: /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/temp/log.do_configure.648
Log data follows:
| DEBUG: SITE files ['endian-little', 'bit-64', 'arm-common', 'arm-64', 'common-linux', 'common-glibc', 'aarch64-linux', 'common']
| DEBUG: Executing shell function autotools_preconfigure
| DEBUG: Shell function autotools_preconfigure finished
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'bit-64', 'arm-common', 'arm-64', 'common-linux', 'common-glibc', 'aarch64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_configure
| checking build system type... x86_64-pc-linux-gnu
| checking host system type... aarch64-fsl-linux-gnu
| checking for aarch64-fsl-linux-gcc... aarch64-fsl-linux-gcc --sysroot=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot
| checking for suffix of object files... o
| checking whether we are using the GNU C compiler... yes
| checking whether aarch64-fsl-linux-gcc --sysroot=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot accepts -g... yes
| checking for gcc... gcc
| checking for aarch64-fsl-linux-readelf... aarch64-fsl-linux-readelf
| checking whether we are using the GNU C++ compiler... no
| checking whether aarch64-fsl-linux-g++ --sysroot=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot accepts -g... no
| checking whether aarch64-fsl-linux-g++ --sysroot=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot can link programs... no
| checking for sysdeps preconfigure fragments... aarch64 alpha arm hppa i386 m68k microblaze mips nios2 powerpc s390 sh sparc tile x86_64
| configure: running configure fragment for add-on libidn
| checking for -fstack-protector... yes
| checking for -fstack-protector-strong... yes
| checking for -fstack-protector-all... yes
| checking for assembler and linker STT_GNU_IFUNC support... no
| checking for gcc attribute ifunc support... no
| checking sysdep dirs... sysdeps/unix/sysv/linux/aarch64 sysdeps/aarch64/nptl sysdeps/unix/sysv/linux/generic sysdeps/unix/sysv/linux/wordsize-64 sysdeps/unix/sysv/linux sysdeps/nptl sysdeps/pthread sysdeps/gnu sysdeps/unix/inet sysdeps/unix/sysv sysdeps/unix sysdeps/posix sysdeps/aarch64/fpu sysdeps/aarch64 sysdeps/wordsize-64 sysdeps/ieee754/ldbl-128 sysdeps/ieee754/dbl-64/wordsize-64 sysdeps/ieee754/dbl-64 sysdeps/ieee754/flt-32 sysdeps/aarch64/soft-fp sysdeps/ieee754 sysdeps/generic
| checking for a BSD-compatible install... /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/hosttools/install -c
| checking whether ln -s works... yes
| checking whether /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/as is GNU as... yes
| checking whether /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld is GNU ld... no
| checking for /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/as... /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/as
| checking version of /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/as... 2.29.1.20170915, ok
| /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld: /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/sysroots-uninative/x86_64-linux/lib/libc.so.6: version `GLIBC_2.27' not found (required by /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld)
| checking for /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld... /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld
| checking version of /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot-native/usr/bin/aarch64-fsl-linux.gcc-cross-initial-aarch64/../../libexec/aarch64-fsl-linux.gcc-cross-initial-aarch64/gcc/aarch64-fsl-linux/6.3.1/ld... v. ?.??, bad
| checking for gnumake... make
| checking version of make... 4.1, ok
| checking for gnumsgfmt... no
| checking for gmsgfmt... no
| checking for msgfmt... no
| checking for makeinfo... makeinfo
| checking version of makeinfo... 6.5, ok
| checking for sed... sed
| checking version of sed... 4.4, ok
| checking for gawk... gawk
| checking version of gawk... 4.1.4, ok
| checking if aarch64-fsl-linux-gcc --sysroot=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot is sufficient to build libc... yes
| checking for aarch64-fsl-linux-nm... aarch64-fsl-linux-nm
| checking for python3... python3
| configure: error:
| *** These critical programs are missing or too old: GNU ld
| *** Check the INSTALL file for required versions.
| WARNING: /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/temp/run.do_configure.648:1 exit 1 from '$cfgscript --host=aarch64-fsl-linux --build=x86_64-linux --prefix=/usr --without-cvs --disable-sanity-checks --with-headers=/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/recipe-sysroot/usr/include --enable-hacker-mode --enable-addons'
| ERROR: Function failed: do_configure (log file is located at /home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/build_s32v234evb/tmp/work/aarch64-fsl-linux/glibc-initial/2.26-r0/temp/log.do_configure.648)
ERROR: Task (/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/sources/poky/meta/recipes-core/glibc/glibc-initial_2.26.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 282 tasks of which 280 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/leon/work/S32V/S32V234EVB/yocto-bsp19.0/sources/poky/meta/recipes-core/glibc/glibc-initial_2.26.bb:do_configure
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

----------------------------------------------------------------------------------------------------------------------------------------

The log said:

'| *** These critical programs are missing or too old: GNU ld
| *** Check the INSTALL file for required versions.'

Which INSTALL file should I check?

Do anybody know how to fix the issue?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,615件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi 2802911181@qq.com,

 

We do not build the linux image for NXP Vision Toolbox for Matlab. Instead we use the one that is shipped with the VSDK 1.2.0.

 

Kushal Shah can you help here?

0 件の賞賛
返信

1,615件の閲覧回数
2802911181
Contributor II

Hi Kushal Shah,  As I didn't find appropriate type, so I selected ' NXP Model-Based Design Tools for VISION'.

0 件の賞賛
返信