Holes for MPL3115A2 Pressure Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Holes for MPL3115A2 Pressure Sensor

4,061 Views
sgdelia31
Contributor I

I'm trying to use the MPL3115A2 barometric/altitude/temperature sensor in a model rocketry project. I know that I'll need to put hole(s) in the side of the rocket in order to get an accurate pressure reading, but I cannot find the size or positioning of those holes in any documentation for the sensor. Does anyone have the information I need or know where I can find it?

The rocket already has four 0.02808 inch holes at 90 degree angles, 4-5 diameter lengths away from the nosecone shoulder for a stratologger, which will also be collecting altitude data. Will those holes be sufficient for the MPL3115A2 sensor as well?

This is the board I'm using for the project, which uses the MPL3115A2 sensor.

https://www.adafruit.com/product/1893 

Thanks!

0 Kudos
Reply
2 Replies

2,474 Views
aliaa12
Contributor I

Great Post! Thank you for visiting here. https://tractorsinfo.com/mysainsburys/ 

0 Kudos
Reply

3,975 Views
mariuslucianand
NXP Employee
NXP Employee

Hello sgdelia31@gmail.com‌,

This community space do not cover the topic you need assistance on.

Please create new thread on the https://community.nxp.com/community/sensors?tid=community  community space or new NXP support case according to following procedure:https://community.nxp.com/docs/DOC-329745.

Kind Regards,

Marius

0 Kudos
Reply