Is there any detailed documentation on how to put together RCW, u-boot image, linux kernel, and root filesystem on a single sd card?
I am working with the LS1046ardb using NXP SDK 2.0. So far I have built fsl-image-minimal and then written the image tmp/deploy/images/ls1046ardb/u-boot-sdcard.bin to sd card with,
sudo dd if=u-boot-sdcard.bin of=/dev/disk2 bs=512 seek=8
This works fine, but I'm wondering why it needs to be written 4K bytes into the sd card. And what other offsets are appropriate for the other components like RCW, linux kernel, and rootfs?
This topic is almost addressed in 3.3.1.8 Programming a New U-Boot, RCW and FMan Ucode on page 38 of
QorIQ LS1046A BSP v0.4, but that section only addresses writing u-boot to sd card - nothing else. It tells me I need to start the u-boot image 8*512 bytes into the card, but doesn't say anything about what can come before or after.
Thanks in advance.
解決済! 解決策の投稿を見る。
I want to follow-up on my own question since it looks like some people occasionally stumble across this.
The layout the sdcard for the LS1046A is as follows:
I want to follow-up on my own question since it looks like some people occasionally stumble across this.
The layout the sdcard for the LS1046A is as follows:
The u-boot-sdcard.bin file contains RCW, PBL and u-boot code. See part of hex dump in the attachment.
The LS1046a boot ROM provides loading from block 8 of the SD card.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------