meta-mingw with sdk2.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

meta-mingw with sdk2.0?

3,789 Views
RandyKrakora
NXP Employee
NXP Employee

Has anyone tried meta-mingw with sdk2.0?

I'd like to build and SDK from yocto ( Linux ) that I can build on a windows PC.

Customer is Aptiv ( Delphi Automotive ).

Regards,

Randy Krakora

Labels (1)
0 Kudos
Reply
3 Replies

3,481 Views
Pavel
NXP Employee
NXP Employee

There is the following information about mingw using in LSDK 1712. See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,481 Views
RandyKrakora
NXP Employee
NXP Employee

I was looking for some guidance to include the meta-mingw layer into Yocto so I could build an SDK for building in Windows for the layerscape parts...

Regards,

Randy Krakora

0 Kudos
Reply

2,934 Views
PeterLendvai
Contributor I

Hi!

Did you manage to build sdk with meta-mingw? I'm interested in too, if you had any luck with it.

Thank you!

0 Kudos
Reply