main-1.0-r0 do_compile: oe_runmake failed while building using bitbake

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

main-1.0-r0 do_compile: oe_runmake failed while building using bitbake

874件の閲覧回数
dibyarekha
Contributor IV

I have created a custom layer as meta-examplelayer. In that layer, I want to compile my application and generate image  for ls1043ardb using bitbake command

Following is my .bb file

DESCRIPTION = "My application"
LICENSE = "MIT"
LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"
 
SRC_URI = "file://main.c \
   file://header.h \
   file://structures.h \
   file://terminalMode.h \
   file://microblaze.h \
   file://Makefile \
   "
CLEANBROKEN = "1"
S = "${WORKDIR}"
 
do_compile() {
 
oe_runmake
 
}
 
do_install() {
install -d ${D}${bindir}
install -m 0755 main ${D}${bindir}
}

 

 

I am getting the following error while bitbake main

ERROR: main-1.0-r0 do_compile: oe_runmake failed
ERROR: main-1.0-r0 do_compile: ExecutionError('/home/icomm/distro/build_ls1043ardb/tmp/work/aarch64-fsl-linux/main/1.0-r0/temp/run.do_compile.59027', 1, None, None)
ERROR: Logfile of failure stored in: /home/icomm/distro/build_ls1043ardb/tmp/work/aarch64-fsl-linux/main/1.0-r0/temp/log.do_compile.59027

ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/icomm/distro/sources/meta-examplelayer/recipes-example/HS_NW/main.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 730 tasks of which 722 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/icomm/distro/sources/meta-examplelayer/recipes-example/HS_NW/main.bb:do_compile
Summary: There were 2 ERROR messages, returning a non-zero exit code.

I have attached the tree of my lmeta-examplelayer and my Makefile

How can I change my .bb file to solve this error.

Please help me out

0 件の賞賛
返信
0 返答(返信)