Use LSDK 17-12 version kernel to bootup ls2088ardb reference board.
Login after about 3mins~5mins, and then 'reboot', the board can not boot up again.
Part log is:
[...
e1000e: EEE TX LPI TIMER: 00000000
reboot: Restarting system
Re
]
The board stops at here.
If login after 15mins or 20mins, the board can boot up well.
Is there anyone has the same issue ?
It seems like I have deleted your reply after I edited to add the attached file(bootlog) ,sorry, I didn't mean it.
It is easy to reproduce, you can try it as well.
I'm not sure it is related to NFS bootway.
Thanks,
Fang
Hello jia fang,
The issue QUBOOT-3723 has already been fixed in the patch [U-Boot] driver: fsl-mc: Perform fsl-mc fdt fixup for lazyapply dpl - Patchwork .
It seems that the reboot problem is related with E1000 Timer, are you using NFS rootfs now?
Would you please provide the whole console log including u-boot, Linux Kernel booting up and the execution of reboot command?
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Oh, I use the flash vbank4 and the lsdk1712 version and find that the issue is still there.
U-Boot 2017.07-g9f7df1b (Dec 23 2017 - 00:31:21 +0800)
SoC: LS2088AE Rev1.1 (0x87090011)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz
CPU6(A72):1800 MHz CPU7(A72):1800 MHz
Bus: 700 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 483038b8 48480048 00000000 00000000
00000010: 00000000 00000000 00a00000 00000000
00000020: 01001180 00002581 00000000 00000000
00000030: 00400c0b 00000000 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 412a0000 00040000
Model: Freescale Layerscape 2080a RDB Board
Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 4
FPGA: v1.22
I tried to update the firmware to LSDK1712 version. then I found the mc bus does not probed.
There should be some problem in MC10.4.0.
The issue is same as the LSDK1712 open issue QUBOOT-3723. So I change to use the 'fsl_mc apply dpl' not the 'lazyapply', the MC works well now.
And it seems like the 'reboot' issue disappear now.