ls1021a-iot booting from SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1021a-iot booting from SPI

1,571件の閲覧回数
renaud
Contributor IV

We have a ls1021A-iot eval board.

I would like to boot it from the SPI NOR. This means I need to change the RCW.

Looking in this git repository: https://source.codeaurora.org/external/qoriq/qoriq-components/rcw/tree/

there is no directory for the ls1021aiot. Where can I find the source? 

I see that s1021aqds/NNR_PSS_NN_60/rcw_1000_qspiboot.rcwhas support for QSPI. Could I use that for the ls1021a-iot?

 

Cheers,

Renaud

 

Cheers,

タグ(3)
0 件の賞賛
返信
6 返答(返信)

1,153件の閲覧回数
Kensou
Contributor III

Did you achieve LS1021A-IOT booting from QSPI? I am trying but with no result

0 件の賞賛
返信

1,148件の閲覧回数
renaud
Contributor IV

yes. On the LS1021A-IOT booting barebox.

0 件の賞賛
返信

1,145件の閲覧回数
Kensou
Contributor III

Could you help me how to do it? I am really struggling but I did not achieve any result.

0 件の賞賛
返信

1,543件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The only officially supported OpenIL boot source is SD card.

If you want to use QSPI boot, you need to modify files in RCW configuration ls1021aqds/NNR_PSS_NN_60/rcw_1000_qspiboot.rcw according to https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/board/freescale/ls1021aiot...

Then generate QSPI RCW image for ls1021aiot.

0 件の賞賛
返信

1,568件の閲覧回数
renaud
Contributor IV
0 件の賞賛
返信

1,569件の閲覧回数
renaud
Contributor IV

I forgot to mention that our final product will boot from parallel NOR.

0 件の賞賛
返信