OpenIL on the LS2028ARDB-PA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenIL on the LS2028ARDB-PA

1,279 次查看
tsn_development
Contributor I

Doing an OpenIL 1.9 build on the LS2028ARDB-PA. Follow instructions in the users manual (V1.9). Used the make on a  fii-ls1028tsn-64b defconfig for an SD card. The sdcard.img file  created sets the DDR memory to 2 GB DDR4, 32-Bit,Cl=11, ECC off. It should be  4 GB DDR4, 32-Bit,Cl=11, ECC on. The boot hangs  because of this. What file needs to be modified in order to set the DDR config correctly?.

0 项奖励
回复
1 回复

1,268 次查看
bpe
NXP Employee
NXP Employee

LS2028ARDB-PA is an invalid part number, so it is not clear what board you are trying to build for. If it is LS1028ARDB-PA, the valid build target for it is nxp_ls1028ardb-64b_defconfig. Building this target should generate all files necessary for SD card boot.  Memory size is detected in  DDR initialization code in TF-A. If you want to know the details, see the code in this directory:

https://source.codeaurora.org/external/qoriq/qoriq-components/atf/tree/plat/nxp/soc-ls1028/ls1028ard...

 

Best Regards,
Platon

 

0 项奖励
回复