I want to use the type6 ,outbound and inbound mode, the p2041 cannot support the
inbound mode, which cpu can support it?
swirte type is more faster than the message type ,such as the type 11.
.
If the p2041 donot support the swrite type , which type can replace the type 6.?
thanks.
Look at the MPC8548, MPC8568/69, P4080 and P5040 processor. See the following document:
http://cache.nxp.com/files/32bit/doc/brochure/PWRARCHQIQSG.pdf?fsrch=1&sr=4&pageNum=1
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks for your reply.
Maybe i mistake the document of the P2041 RM.
Now I can use the swrite inbound mode using the DMA.
when I write data using the swrite outbound, the target received the data, which shows the data type is type5 nwrite.
I donot know the reason.