how to use the srio type6 swrite mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use the srio type6 swrite mode?

2,134件の閲覧回数
yinux
Contributor III

I want to use the type6 ,outbound and inbound mode, the p2041 cannot support the

inbound mode, which cpu can support it?

swirte type is more faster  than the message type ,such as the type 11.

.

If the p2041 donot support the swrite type , which type can replace the type 6.?

thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,790件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the MPC8548, MPC8568/69, P4080 and P5040 processor. See the following document:

http://cache.nxp.com/files/32bit/doc/brochure/PWRARCHQIQSG.pdf?fsrch=1&sr=4&pageNum=1


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,790件の閲覧回数
yinux
Contributor III

thanks for your reply.

Maybe i mistake the document of the P2041 RM.

Now I can use the swrite inbound mode using the DMA.

when I write data using the swrite outbound, the target received the data,  which shows the data type is type5 nwrite.

I donot know the reason.

0 件の賞賛
返信