how to use the srio type6 swrite mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use the srio type6 swrite mode?

2,132 次查看
yinux
Contributor III

I want to use the type6 ,outbound and inbound mode, the p2041 cannot support the

inbound mode, which cpu can support it?

swirte type is more faster  than the message type ,such as the type 11.

.

If the p2041 donot support the swrite type , which type can replace the type 6.?

thanks.

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,788 次查看
Pavel
NXP Employee
NXP Employee

Look at the MPC8548, MPC8568/69, P4080 and P5040 processor. See the following document:

http://cache.nxp.com/files/32bit/doc/brochure/PWRARCHQIQSG.pdf?fsrch=1&sr=4&pageNum=1


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,788 次查看
yinux
Contributor III

thanks for your reply.

Maybe i mistake the document of the P2041 RM.

Now I can use the swrite inbound mode using the DMA.

when I write data using the swrite outbound, the target received the data,  which shows the data type is type5 nwrite.

I donot know the reason.

0 项奖励
回复