Was working on lsdk 19.09 for imx6qsabresd .
When using [root@fbubuntu flexbuild_lsdk1909_update_221019]$ flex-builder -m imx6qsabresd
got an error while the build was at
"Building the dependent build/linux/kernel/arm32/IMX/uImage ... "
Error
*** Can't find default configuration "arch/arm/configs/imx_v7_defconfig"!
So copied one of the defconfigs named "imx_v6_v7_defconfig" to "imx_v7_defconfig"
Again started the build ,but now getting the following error
build/firmware/u-boot/imx6qsabresd/imx6qsabresd_boot.scr [Done]
INSTRUCTION: mkbootpartition
DESTARCH: arm32
PORTFOLIO: IMX
CONFIGLIST: build_lsdk.cfg
INSTRUCTION: mklinux
DISTRO TYPE: yocto
DISTRO SCALE: tiny
DESTARCH: arm32
PORTFOLIO: IMX
CONFIGLIST: build_lsdk.cfg
FATAL ERROR: Couldn't open "../../build/linux/kernel/arm32/IMX/imx7ulp-evk.dtb": No such file or directory
Unable to Proceed further
Hello Madhusudan Kumar R,
I have moved this thread to the layerscape community. They may be able to provide better guidance on how to port the lsdk to the i.MX, if possible, as they are more familiar with this sdk.
My apologies for the inconvenience.
Regards,