Hi,
When i try to connect code warrior tap to LS1046ardb , I am getting the following error.
Kindly help
Which Target Configuration is selected?
Run Diagnose Connection:
Press "Connection Diagnostics" button and provide the Connection Diagnostics tab screenshot.
Please try the following steps:
1) completely uninstall CodeWarrior IDE
2) disable anti-virus application(s)
3) install latest Java
4) install CodeWarrior IDE
5) enable anti-virus application(s)
In case of further questions capture complete Help message as text.
After disabling the anti virus and reinstalling the code warrior , it is working fine.
Thank you.