Using TSECx SerDes as a SGMII and ECx pins as GPIO in LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using TSECx SerDes as a SGMII and ECx pins as GPIO in LS1021A

752 Views
senoghte
Contributor II

Hi eyery body
Can I use eTSEC1 or eTSEC2  in SGMII mode beside of using Ethernet Controller Pins that including EC1_GTX_CLK ,
EC1_TX_CLK, EC1_GTX_CLK125 ,EC1_RX_ER, EC1_RXD[0:3] and EC1_TXD[0:3]  as GPIO at the same time?
Regards

Labels (1)
0 Kudos
Reply
1 Reply

609 Views
alexander_yakov
NXP Employee
NXP Employee

Please look LS1021A Reference Manual, Table 3-1.

For example, pin "EC1_GTX_CLK" alternate functions are:

GPIO3_07
EC1_TX_CLK
SAI2_TX_BCLK
FTM1_EXTCLK

That is - pin EC1_GTX_CLK can be configured as GPIO. This configuration can be done via RCW, please look Table 4-14, fields "EC1", "EC2", "EC3". Note - all pins, listed in one field, can be configured only simultaneously.

The same for other pins in your list.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply