Hi eyery body
Can I use eTSEC1 or eTSEC2 in SGMII mode beside of using Ethernet Controller Pins that including EC1_GTX_CLK ,
EC1_TX_CLK, EC1_GTX_CLK125 ,EC1_RX_ER, EC1_RXD[0:3] and EC1_TXD[0:3] as GPIO at the same time?
Regards
Please look LS1021A Reference Manual, Table 3-1.
For example, pin "EC1_GTX_CLK" alternate functions are:
GPIO3_07
EC1_TX_CLK
SAI2_TX_BCLK
FTM1_EXTCLK
That is - pin EC1_GTX_CLK can be configured as GPIO. This configuration can be done via RCW, please look Table 4-14, fields "EC1", "EC2", "EC3". Note - all pins, listed in one field, can be configured only simultaneously.
The same for other pins in your list.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------