Use Tamper Detect (TA_TMP_DETECT_B) as GPIO in LS1027A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use Tamper Detect (TA_TMP_DETECT_B) as GPIO in LS1027A

ソリューションへジャンプ
1,083件の閲覧回数
igor_franco
Contributor IV

Hello,

I am working on a customized board with the LS1027AE processor and want to use the Tamper Detect pin as a GPIO to interrupt the processor.

Is this possible? If yes, what are the GPIO group and pin values that represent the Tamper Detect pin?

P.s.: I read in the datasheet that this pin has no additional function. I only want to confirm if it is possible or not.

Best regards,

Igor

0 件の賞賛
返信
1 解決策
1,075件の閲覧回数
ufedor
NXP Employee
NXP Employee

> I read in the datasheet that this pin has no additional function.

This is correct - i.e no way to use the pin/signal as GPIO.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,069件の閲覧回数
igor_franco
Contributor IV

Thank you for the fast answer.

0 件の賞賛
返信
1,076件の閲覧回数
ufedor
NXP Employee
NXP Employee

> I read in the datasheet that this pin has no additional function.

This is correct - i.e no way to use the pin/signal as GPIO.

0 件の賞賛
返信