Hello,
I am working on a customized board with the LS1027AE processor and want to use the Tamper Detect pin as a GPIO to interrupt the processor.
Is this possible? If yes, what are the GPIO group and pin values that represent the Tamper Detect pin?
P.s.: I read in the datasheet that this pin has no additional function. I only want to confirm if it is possible or not.
Best regards,
Igor
Solved! Go to Solution.
> I read in the datasheet that this pin has no additional function.
This is correct - i.e no way to use the pin/signal as GPIO.
Thank you for the fast answer.
> I read in the datasheet that this pin has no additional function.
This is correct - i.e no way to use the pin/signal as GPIO.