Raw SerDes Usage on LX2160A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Raw SerDes Usage on LX2160A

ソリューションへジャンプ
899件の閲覧回数
reyesc
Contributor I

Hopefully this isn't too broad of a question (and is in the appropriate place).

I'm currently investigating transferring raw data via SerDes and was hoping someone could point me to some documentation/resources that might help out. Churning through the available docs I see that it's tied pretty tightly to the various protocols (ethernet, pcie, sata, etc) via dpaa2 and I haven't seen much in terms of utilizing the SerDes sans-protocol.

The use case here is pretty basic. At some point in the future the plan is to utilize the 25G and PCIe lanes, however currently the hardware won't be in place and so I'd just like to send some raw data out to verify our connections to those paths coming out of the chip. Basically, a loop-back test.

For what it's worth we're running LSDK 18.04.

Any help/info/guidance would be greatly appreciated. Let me know if more info is needed.

0 件の賞賛
返信
1 解決策
814件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
862件の閲覧回数
Irene
NXP Pro Support
NXP Pro Support

There is an application note on our website that might help answer some questions for you. 

https://www.nxp.com/docs/en/application-note/AN13329.pdf

0 件の賞賛
返信
815件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

0 件の賞賛
返信