Platform: LX2160A customized board card。and my ddr4 is discrete type.
I did the validation with QCVS, then what should I do to use the calibrated value.
已解决! 转到解答。
This should be the code for the slave core, entering into sleep mode. Please attach to the master core to check the problem code.
在原帖中查看解决方案
Please refer to section "1.1.1.2 Configure DDR controller" in the attached QCVS DDRv user guide.
After creating a QCVS DDR project for Discreate DRAM with the default parameters, please fill "Properties" panel according to your DDR Datasheet.
hi yipingwnag:
how to use codewarrior to debug uboot ? my pbl It's already ok, but my uboot can not start up.
Please refer to https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-bo...
hello.
when i debugging uboot with codeworrior, my uboot is wrong here: cbz x0, slave_cpu.
What does the mean of "slave_cpu", What cause the wrong here?
thanks.